AXIS#.IL.COGCOMP.MOVETOSTART.MOVE
Description
Moves the axis to the Teach Start Position (AXIS#.IL.COGCOMP.TEACH.POSSTART) using the specified acceleration (AXIS#.IL.COGCOMP.MOVETOSTART.ACC), deceleration (AXIS#.IL.COGCOMP.MOVETOSTART.DEC) and velocity (AXIS#.IL.COGCOMP.MOVETOSTART.V).
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-08-00-000 |
General Information
|
Type |
Action |
|
Units |
N/A |
|
Range |
N/A |
| Default Value | N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.COGCOMP.TEACH.MOVETOSTART.MOVE | 0x500A | 0x?? | UINT | 1:1 | - | W | False |
| AXIS2.IL.COGCOMP.TEACH.MOVETOSTART.MOVE | 0x510A | 0x?? | UINT | 1:1 | - | W | False |